0
0 Items£0.00
ex VAT

Fans & Air Conditioners

Reliable and Efficient Cooling Solutions

At CPC we make keeping cool and comfortable both easy and cost-efficient with a selection of fans, air conditioners and dehumidifiers, ideal for the home, office, or workshop.

Air Conditioners

Air Conditioners

Dehumidifiers

Dehumidifiers

Air Purifiers

Air Purifiers

Fantastic Deals

Shop by Fan Type

Desk Fans

Desk Fans

Super value fans ranging from 290mm to 600mm in diameter.

High Velocity Fans

High Velocity Fans

Great for cooling and ventilating workshops, garages and indoor spaces.

Pedestal Fans

Pedestal Fans

Modern, sleek designs with height adjustable options for flexible use.

Tower Fans

Tower Fans

Awesome oscillating fans with a slim, space-saving design.

Outdoor Heaters

Popular Brands

AIR X PRO
PRO-ELEC
AIRCONDITIONINGCENTRE
CLARKE INTERNATIONAL
MEACO
DEWALT
Some interesting questions…
  • Pedestal fans generally come on a height-adjustable stand and can be positioned at a height suitable to the user's requirements, while Tower fans normally have a long rectangular outlet, with the bottom part positioned closer to the floor.

  • Once air has been drawn into the unit, the air conditioner compresses and liquefies it before cooling the air in a condenser and allowing it to expand through an evaporator. The unit then re-circulates the air into the room in a cooler state, or at a warmer temperature if using the air conditioning unit in reverse mode. Simple!

  • Working in a similar way to a thermostat, a humidistat will trigger the dehumidifier to start working once humidity levels reach a certain point.

  • The British thermal unit (or BTU) usually measures an amount of energy, whereas watts measure the rate that energy is transferred so they don't directly equate to the same thing. A BTU is a traditional unit of energy used to represent the amount of energy needed to heat 1 pound (0.454kg) of water by 1°F (0.556°C) and is commonly used in the power, steam generation, heating, and air conditioning industries. Below is a typical scale of BTU vs. watt

    1 watt = 3.41214 BTU/h

    1000 BTU/h = 293 watt’s

  • Air coolers and air conditioners will often have oscillating louvres, which move allowing the air to be directed in different directions rather than solely on a fixed point.

  • BTU is a unit of energy, which stands for British thermal units. One BTU relates to the amount of energy needed to raise the temperature of one pound of water by 1°F. Energy is more commonly measured in Joules with one BTU equivalent to approximately 1055 joules. Wish you'd never asked? Thought so.

  • It's a discrete fan designed for use at your desk, which plugs into the USB port on your PC or laptop. It takes up less room than a conventional desk fan and is a cost-effective way of keeping cool at work. You can view our selection of USB desk fans by clicking here.